Como o podemos ajudar hoje?

Which base units are compatible with XVUZ12 installation in XVU range?

The compatibility of XVUZ12 in XVU range as below:
XVUZ02, XVUZ02Q, XVUZ03, XVUZ400, XVUZ800, XVUZ05.