Issue
The AccuSine+ can be used as a harmonic filter and power factor correction/Load balancing simultaneously. The total output current will be limited by harmonic current and the reactive current.
Product Line
AccuSine PCS+
Resolution
The total output of the harmonic filter in dual mode is governed by the following formula:

When the total current output of the active filter required exceeds the unit rating, the AccuSine PCS+ has a harmonic priority setting to determine which mode has priority.
Use percentage of harmonic priority to set output current split
The AccuSine+ can be used as a harmonic filter and power factor correction/Load balancing simultaneously. The total output current will be limited by harmonic current and the reactive current.
Product Line
AccuSine PCS+
Resolution
The total output of the harmonic filter in dual mode is governed by the following formula:
When the total current output of the active filter required exceeds the unit rating, the AccuSine PCS+ has a harmonic priority setting to determine which mode has priority.
Use percentage of harmonic priority to set output current split
- 100% means output capacity utilized for harmonic correction, then left over can be used for Power factor correction.
- 0% assigns fundamental (PF correction) current as the primary mode, left over used for harmonic correction.
Publicado para: Schneider Electric Portugal


Precisa de ajuda?
Ferramenta de seleção de produtos
Encontre rápida e facilmente os produtos e acessórios certos para as suas aplicações.
Obter um Orçamento
Inicie o seu pedido de contacto online e um especialista irá contactá-lo.
Onde adquirir?
Encontre facilmente o distribuidor mais próximo da Schneider Electric perto de si.
Centro de ajuda
Encontre recursos de apoio para todas as suas necessidades, num único local.