Como o podemos ajudar hoje?

How to check Heat Tag and communication gateways on Smart solutions tab in NL 4.9.3 version of Ecodial .

Steps to check Heat Tag and communication gateways in Smart solution tab in Ecodial :
STEP-1 Launch Ecodial 4.9.3 NL version of Ecodial
STEP-2 Create a network with 50, 100 and 200A load.
STEP-3  Run the calculation
STEP-4  GO to Smart solution tab
STEP-5 Under fire prevention tab  select the required circuit breaker & switchboards to be protected
STEP-6 Run Smart solution by clicking “ SMART SOLUTION” TAB
STEP-7 Smart solution results will appear as below :
Under  “Electrical Fire prevention” solutions check there exists heat tags and communication gateways for the respective switchboards which is  required  for fire prevention.
STEP -8 Follow the instruction which application is suggesting in “ Electrical  Fire prevention “tab.
STEP-9  After following the instruction by adding add on RCD go to “ smart solution tab “ and again “ Run smart solution”
STEP10 – Network will charge out “ Heat  tag solution and communication gateways “ for respective circuit breakers and switchboard as below: