Ovaj dokument je aktuelan, ali može da navodi zastarele proizvode.

How technology can help advance green hydrogen initiatives. White Paper

New technologies will pave the way as the world moves away from fossil fuels and towards renewable energy sources. Green hydrogen is one of the emerging, enabling technologies that will facilitate the transition away from hydrocarbons. Still, it is in its infancy, and determining how to achieve cost-effective production presents a formidable challenge. Finding the forward path towards efficient green hydrogen production requires new technologies and new thinking. The solution is on the horizon, but for the industry to reach this ambitious objective, it must recognize the essential role digitalization will play in changing the status quo.

Reference

 : 

Datum

 : 

Tip

 : 

Jezici :

Verzija :

Fajlovi
Size
998-21792107_GreenHydrogen_GMA_eWhitePaper (.pdf)

Asortimani proizvoda:

IEC 61850 Standard, SET IEC 61850 System Engineering Tool

Otključavanje dodatnih funkcija

Prijavite se ili se registrujte da biste videli dodatne funkcije

loader-lg loader-sm