{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Is it possible to rotate the DMCR or DGPT2 protection in Oil Distribution...

It is possible in Oil Distribution Transformers, but can only be done by an authorised service. Please consult to Schneider since unauthorised attempt will cause warranty loss.

iDisplay Touch screen drivers for W 7 32 and 64 bits

Drivers Windows 7 for iDisplay iDisplay Touch screen drivers for W 7 32 and 64 bits Goals and Symptoms Currently, our iDisplays are supplied only with the Windows XP drivers for Touch screen. The...

Could you clarify the meaning of "PUP" in the Comtrade file of SFT2826?

PUP is the "pick-up" of the fault. Often people mistake "PUP" as the pickup of disturbance recording, but this is incorrect because the disturbance recording is often configured...

Logipam (SFT2885) Manual for Sepam Series 80

Issue: This document can be useful to understand how to use and test the Logipam Software (SFT2885) for Sepam Series 80 Relays. Product Line: Sepam Series 80 Relays Environment Cause This article...

M340 Email

Goals and Symptoms Sending an Email from the embedded Ethernet port on a M340 CPU. Facts and Changes NOTE: The send Email function can only be used on the Embedded Ethernet port of the M340 CPU...

Can we upload programs with Vijeo Designer from the Magelis XBTG/GK/GT,...

Goals and Symptoms Can we upload programs with Vijeo Designer from the Magelis XBTG/GK/GT, HMIGK/GTO/GTU, HMISTO/STU? Causes and Fixes It is necessary to previously configure the Vijeo-Designer...

Is it possible to operate motor by VSD if motor rated voltage is greater...

THere is one fact, than ATV output voltage can be regulated from zero to the max value that corresponds to ATV input voltage. So if you use 400V supply the max voltage at the ATV output can be 400V....

What is the color code pinout for the BMXFTW308S ?

Title The color code pinout applies to all the BMXFTWx08S cable lengths. Issue Product Line Modicon M340 Environment Cause Resolution See the attached diagram

Popular Video FAQsPopular Videos

video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail

Learn more through our Generic Knowledge FAQsGeneral Knowledge

What’s AC-3e rating means and what’s their application ?

AC-3e rating is the capability of the contactor for starting and switching off high efficiency squirrel cage asynchronous (IE-3/ IE-4) motors during running and reversing operations, which have...

How to establish the communication with S7-1500 PLC if using TIA Portal...

In PLC side: 1.Use TIA Portal V11-V16 to configure the PLC communication settings. 2.Select the PLC and enter the correct version of the firmware (We can check for the firmware version of the PLC in...

What are the effects of dV/dt on a Motor when using a VSD?

As there is an impedance mismatch at the termination of the motor cable to the motor, there will be a reflected wave which travels back along the motor cable causing overvoltage’s. Overvoltage’s on...

How to disable the system error popup window in Vijeo Designer?

Please refer to the setting in the following picture: The setting gives you the option to turn system error window on or off. Select Yes to show system error message window on the panel at runtime....

Failure of Exporting CID/ICD file

Issue When customer want to export CID/ICD file from our Easergy P3 relay, it is showing an alarm(as the below picture), and fail to export CID/ICD file....

What are the coil control voltages available for TeSys Giga ?

TeSys Giga contactor is available in advanced version and standard version. Both advanced and standard version have different type of control voltages. Advanced version Standard version 24…48V AC/DC*...

Is it possible to downgrade the EOTE project?

No, It is not possible to downgrade the EOTE project to an older version. But when we upgrade the original project, for example, when we upgrade the project from EOTE 3.1 SP1A to EOTE 3.2, EOTE will...

What are the different protections available in TeSys Giga electronic...

TeSys Giga LR9G electronic overload relays provide: Wide range of overload protection (0.25…1x Ir setting with 64 step dials for accuracy) Phase imbalance protection (Can be switched ON/OFF) Ground...