Saudi Arabia
Welcome to the Schneider Electric Website

Welcome to our website.

You can choose another country to view available products or go to our Global website for company information.

Choose another country or region
  • Default Alternative Text

    Press

Schneider Electric Introduces Altivar Process, the First Ever Variable Speed Drive with Embedded Services

04.06.2015
The Range of Drives Serves for Industrial Applications

Riyadh, KSA – June 07, 2015 - Schneider Electric™, the global specialist in energy management™, today announced the release of Altivar® Process – a range of drives for process applications from 0.75kW to 1.5MW. It is the first variable speed drive on the market with embedded intelligent services.

Thanks to a convergence of IT and OT technologies, Altivar Process drives deliver added value services in the Water, Oil & Gas, MMM, and Food & Beverage industries that enable business and process optimization through improved life-cycle asset management and optimized energy consumption.

The launch is scheduled on 10th June, 2015 at the Marriott Hotel, Riyadh, where senior executives from Schneider Electric will offer insights into the new product during the event that is anticipated to attract end users, government officials, consultants, original equipment manufacturer (OEM), contractors, etc.

Optimized business performance

Through advanced system and equipment condition monitoring, Altivar Process ensures that applications are performing at optimum efficiency at all times. Compared to conventional drives, Altivar Process delivers an additional 8 percent cost reduction thanks to its ability to instantly detect efficiency drifts and to monitor motor power with a high level of accuracy (<5%). This enables the automation system to immediately make adjustments, thereby minimizing a negative impact on the bottom line. In contrast to conventional drives, Altivar Process is also able to reduce downtime by another 20 percent due to predictive, condition-based maintenance and an innovative user-interface with easy-to-understand graphs.

Process visibility and real-time intelligence

Fully integrating both architecture and business systems, Altivar Process provides process visibility and transparent access to enriched data at both the factory and asset level. Embedded Ethernet and advanced web servers provide consistent and secure access to this information, anytime and from anywhere. The embedded web server allows users to select which information to view and which to store (datalogging). Additionally, KPIs and alarms are automatically monitored and can generate alerts to system operators of any performance irregularites so preventive steps can be taken to maintain optimum process efficiency and profitability.

Unique design reduces maintenance

Compact, modular, and flexible, Altivar Process fits any application and is simple to install and integrate, whether in new installations, retrofits, or upgrades. Designed for critical applications, it is uniquely engineered and integrates process, grid, and installation into a complete solution that reduces maintenance requirements and TCO. In addition, its compact, modular, and low-weight modules simplify spare parts inventory and reduce repair time (cooling fans mount in just 5 mins).

To further simplify maintenance, enhance troubleshooting, and reduce downtime and its related costs, operators can access technical documentation, support, and diagnostic information directly on their mobile devices. Error messages also generate dynamic QR codes for instant access to comprehensive support information to efficiently solve issues right on site, while QR codes printed directly on the drives provide instant access to customer care centres and online troubleshooting.

A green drive from beginning to end

Even at the end of its useful life, Altivar Process drives are a green solution since 70% of its components parts can be recycled. And, because they carriy the “Green Premium” label - Schneider Electric’s unique eco-brand signifying products that meet the European RoHS directive and REACH regulations – Altivar Process drives go beyond compliance regulations of today and help to the environmental regulations of tomorrow.
Chat with us

Do you have questions or need assistance? We’re here to help!