Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the meaning of the Speed-range ratio in Altivar 61/71 Range Drives.

The Speed-range ratio for Drives is 20:1, 100:1 or 1000:1. This is an indication of how slow the Drive can run the motor, before the motor starts to overheat.

Drive with a 1000:1 ratio is good, as compared to 20:1 or 100:1.
The Altivar 61 and Altivar 71 Range of Drives have the Speed-range ratio of 1000:1 in closed loop and 100:1 in open loop operation.
Example:
The speed in RPM (Revolutions per Minute) of a 4 pole, 50 Hz Motor will be 1500 RPM.
If the Drive Speed-range is 1000:1, Drive can run the motor as slow as 1.5 RPM (1500/1000 = 1.5) without overheating.
For 100:1 it is 15rpm and for 20:1 it is 75rpm.
The higher the Speed-range ratio, the slower the motor can be operated safely without overheating.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings