Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why is my Share-UPS is sending a low battery signal to the attached devices?

Issue

My Share-UPS is sending a low battery signal to the attached devices.


Product Line

Share-UPS - AP9207


Environment

• All firmware versions
• Specific configurations listed below


Cause

There are several reasons why the Share-UPS could force a low battery signal to the attached servers even though the UPS does not have a low battery. See below for a resolution.


Resolution

Refer to the possible causes and resolutions listed below.


What serial cables are being used by the Share-UPS?
The server attached to the advanced port should be connected to the Share-UPS using a black cable with part number 940-0024 or 940-1524. The remaining servers should be attached to the Share-UPS using a gray cable with part number 940-0020. PowerChute Plus or Powerchute Business Edition on these ports with a UNIX based system would require the 940-0023A cable. If any other cable is used, a low battery or on battery signal will be generated.
What mode is the Share-UPS in?

The dip switches on the front of the Share-UPS determine which shutdown mode the device will use. The three modes are Confirmed, Timer, or Low Battery. Use the position of the dip switches and the table located on the top of the Share-UPS to determine which mode the Share-UPS is in.
If the Share-UPS is using Confirmed Mode a low battery signal is sent when:
  • The UPS reaches a low battery condition.
  • A user logged into the management port of the Share-UPS and commanded it to shutdown the load.
  • The UPS went to battery and forced the Smart Signaling server to shutdown.
  • Once the Smart Signaling server is shutdown, the Share-UPS forces a low battery signal to all the attached servers.
If the Share-UPS is in Timer mode a low battery signal is sent when:
  • The UPS reaches a low battery condition.
  • The timer being used by the Timer Mode expired (See the Share-UPS User's Manual for more details).
  • A user logged into the management port of the Share-UPS and commanded it to shutdown the load.
  • The UPS went to battery and forced the Smart Signaling server to shutdown. Once the Smart Signaling server is shutdown, the Share-UPS forces a low battery signal to all the attached servers.
If the Share-UPS is configured for Low Battery Mode than a low battery signal is sent when:
  • The UPS reaches a low battery condition.
  • A user logged into the management port of the Share-UPS and commanded it to shutdown the load.
  • The UPS went to battery and forced the Smart Signaling server to shutdown. Once the Smart Signaling server is shutdown, the Share-UPS forces a low battery signal to all the attached servers.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings