Issue
Network Management Card - Single Phase Symmetra SNMP Trap #77 details
Product Line
- UPS Network Management Card 1 - AP9617, AP9618, AP9619
- UPS Network Management Card 2 - AP9630/AP9630CH, AP9631/AP9631CH
Environment
- All serial numbers
- All firmware versions
- SNMPv1 or v3 traps
Cause
SNMP trap # 77 (abnormalCondition) is reserved for specific UPS failures. When trap #77 is sent, it also has a binded subtrap which gives further detail into the nature of the fault. The subtraps are specific to the UPS family type.
Resolution
Attached is a breakdown for the Symmetra single phase line of UPS (Symmetra RM, Symmetra LX, Symmetra Power Array), which uses the Network Management Card APP called 'sy'.
Released for: Schneider Electric Saudi Arabia


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.