Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
IP Installer Utility for APC KVMXXXX Digital IP KVM Switches

Issue

IP Installer provided for user download in order to configure/modify TCP/IP settings for APC KVMXXXX Digital IP KVM switches


Product Line
  • Rack Accessories - KVM Switches
    • KVM1116P
    • KVM2116P
    • KVM2132P

Environment

  • All serial numbers
  • KVMs connected via network


Cause

One option for users to assign TCP/IP settings is to use the attached IP Installer .exe on Windows systems to locate APC KVMXXXX Digital IP KVM Switches via the network. This tool requires that the "IP Installer" setting in Device Management menu is set to Enabled. If the setting is set to View, the user can search and identify the KVM but not modify TCP/IP settings. If the setting is set to Disabled, the KVM switch will not be discovered by the utility.


Resolution

Download the attached .exe file in order to utilize the tool. Alternatively, a user can connect a keyboard, monitor, and mouse to log in and configure the KVM switch as well.

Schneider Electric Saudi Arabia

Attachment(s)
APC_IPInstaller_KVMXXXX.exe [336 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings