Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ACSC Compressor Not Turning On
Issue:
What are the causes that will keep a compressor from turning on to a ACSC100 cooling unit.
Product line:
ACSC100
Environment:
All Serial Numbers
Cause:
Start Up/Install
Resolution:
With an ACSC100 set for spot/discrete mode, please check the system pressure. Please note standing pressure of R410a @ 70 degrees is approx. 201 psi. Therefore, if the standing psig reading on the unit is 41 psi, for example, the refrigerant has obviously fractionated to be at 41 psi. Per the unit’s firmware if the pressure is below 90 psi the unit will not start compressors, nor annunciate any alarms to the contrary.

A couple of things that will keep the SC compressor from starting are:
  • If the Suction Pressure is below 92psi then the compressor will not start, and there are no alarms reported on this.
  • If the pressure difference between the suction and discharge pressure is above 7psi then the compressor will not start, and no alarms are reported. The unit will log an event that reads "Startup Line Pressure Imbalance."


Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings