Issue:
What are the lengths of the DC cables that are attached to single phase Symmetra extended run (XR) frames?
Product Line:
Single Phase Symmetra XR Frames
Environment:
All serial ranges
Cause:
These products are designed to be able to reach each other if position in the same area. This information can be relevant if a user is planning on installing the products in slightly different areas - different racks, for example.
Resolution:
The following table outlines the cable lengths of the DC cable provided with each of the single-phase Symmetra Extended Run cabinets.
XR Type | Cable Type and Length |
SYXR4 | Fixed or Detachable 5ft (1.5m) |
SYXR12 | Fixed or Detachable 5ft (1.5m) |
SYRMXR4 | Fixed 2ft (0.6m) |
SYARMXR3 | Fixed 3.5ft (1.0m) |
SYARMXR9 | Fixed 5ft (1.5m) |
SYAXR9 | Fixed 5ft (1.5m) |
Released for: Schneider Electric Saudi Arabia
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.