Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Using a UPS with X-10 Equipment

Article available in these languages: Thai

Issue:

X-10 technology is a home control system that sends high frequency electrical signals that ""piggy-back"" the AC line to control common household items such as lights and appliances.

Product Line:

SurgeArrest, Back-UPS and Back-UPS PRO

Environment:

N/A

Cause:

APC devices are designed to filter out EMI (Electro Magnetic Interference) and RFI ( Radio Frequency Interference), which the X-10 technology appears to be when applied to the device.

Resolution:

The use of such technology does not adversely affect APC UPSs. However, a UPS or surge suppressor may absorb or filter out X-10 signals as UPSs and suppressors treat these signals as noise. The result, then, is that some X-10 equipment may cease to receive signals.

A possible solution is to install an X-10 isolator which prevents a UPS from filtering out these signals. One commercial solution is currently available from www.SmartHome.com. It is called a "noisy device filter".

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings