Issue:
PowerChute Personal Edition v3.0, 3.0.1, 3.0.2 : Installation says the Data Service failed to start
Product Line:
PowerChute Personal Edition (PCPE) version 3.0, 3.0.1, 3.0.2
Environment:
All supported Windows OS
Cause:
This issue happens if you do not have the latest service pack of .Net 2.0.
Solution:
1. Open up the Control Panel
2. Go to Programs and features
3. In the left panel select Turn Windows features on or off
4. From the list select Microsoft .NET Framework 3.5.x and then click ok. Windows will install the service
NOTE: PCPE 3.1 requires .NET 4.0
Released for: Schneider Electric Saudi Arabia


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.