Issue:
Modbus communication on a Uniflair unit.
Product line:
Uniflairl.
Environment:
All Models and Serial Numbers.
Cause:
Install.
Resolution:
MODBUS RTU
Scenario 1
Modbus is a communication protocol very famous and used all over the world. It’s quite easy and not so structured.
• It has been developed at the end of ’70 from Modicom
• The communication is multidrop, with Master and Slaves
• It is not used only with industrial application
• Serial communication: RS232 or RS485 half duplex
• Protocol type: Modbus RTU (1 byte = 2 hexadecimal words) and Modbus ASCII (1 byte = 2 ASCII words).
Configurable Baud rate (max 19200)
The units, all fitted with the serial card, are connected:
• each unit with the RS485 cable;
• last unit with the final resistor;
• first unit with the Gateway.
To realize a local net to be connected to a BMS working with Modbus, it’s necessary:
• 1 gateway LBM every 16 units;
• 1 serial card RS485 for every controller;
• 1 terminal line (120 Ω);
• PC for the gateway configuration.
Scenario 2
Units fitted with pCO1, upCOxs
To realize a local net to be connected to a BMS working with Modbus, it’s necessary:
• 1 RS485 serial card for every controller;
• 1 terminal line (120 Ω);
• PC for the gateway configuration.
Released for: Schneider Electric Saudi Arabia


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.