Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How deep must the AR7580A Cable Manager be installed so the AR7581A Hinged Cover can open 90 degrees?
Issue:
Need to make sure the cover opens far enough to install and maintain cables.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Customer needs to be able to fully open the hinged cable cover to add, move or change cables.

Resolution:
The AR7580A cable manager needs to be installed at least 10.5" deep in order for the AR7581A hinged cover to open a full 90 degrees.
Also see attached file for photo.

Schneider Electric Saudi Arabia

Attachment(s)
20140115 AR7580A Installation Depth.pdf [362.29 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings