Issue
User would like to know the information contained in the Sepam series 80 memory cartridge
Product Line
Sepam series 80
Environment
Memory cartridge
Resolution
*Warning: The cartridge must not be removed while Sepam is energized*
The Sepam series 80 cartridge contains the following information:
- System and application software (protection functions, protection and parameter settings)
- Customized monitoring and control functions (matrix, equation editor, customized logic schemes..)
- Customized working language
Released for:Schneider Electric Saudi Arabia