Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the meaning of the error code 'FFFF' on the READ_REG_QX Function Block Status pin?

This error code is not documented but indicates that the Quantum 140CRP31200 module does not have a minimum firmware version of 1.56. For BMXCRA31210 with BMXNOM0200 communications on a QEIO network, the Quantum 140CRP31200 module requires at least the firmware version of 1.56.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre