The default StatusRegister setting of 1100 will work with the Power Meter 600 in PowerLogic SCADA, even though 1100 is not defined in the PM6 Register List. If the user reads register 1100 with a generic Modbus register reader, he will receive a value of 32768. While this denotes an undefined value, the register is still readable and therefore, the PM6 I/O device can use this register as verification to come online.
The following is some additional general information about the StatusRegister parameter:
This parameter defines the address of the register that the driver will read to determine whether a device is responding to communication requests. The result of this read is not important; however, it must be a valid register address within the device. This parameter can only be configured for the PWRMODBUS driver.
Keywords: Series 600, PM600, PM620, PM650
Legacy KB System (APS) Data: RESL203061 V1.0, Originally authored by AnVa on 08/06/2010, Last Edited by AnVa on 08/06/2010
Related ranges: PowerLogic SCADA 7.1
Released for: Schneider Electric Saudi Arabia








Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.