undefined [object Object]
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How To Add Icons and how To Create A New Customized Toolbar

Issue
The purpose of this resolution is to provide instructions on how to create a customized toolbar and add icons
to the new customized toolbar in ProWORX 32,

Product Line
ProWORX 32

Environment
Windows 7, 10

Resolution
The following procedure can be used to create a new customized toolbar inProWORX 32.

  • Right click on the toolbar and select customize.

Customize toolbar
  • Click on the 'New' button.

New button
  • Type in a name for the new toolbar.
  • Click on the 'OK' button

New name
  • Closeout the 'Customize' window by clicking on the 'Close' button..

Customize
  • Drag the new toolbar icon and reposition it on the menu bar space.

Click


Right click
  • Right click on the added toolbar icon and select customize.

Customize
  • Click on the 'Commands' tab

Commands
  • Click on an item in the 'Categories' list.
  • Click on the icon in the 'Commands window and drag the icon over to the new toolbar.

Customize

Customize icons
  • The following figure shows the icon added to the new toolbar.

New toolbar

Schneider Electric Saudi Arabia