Issue
Does Vijeo Designer link to individual bits from an INT or DINT using the RSLogix 5000 L5K file?
Product Line
Vijeo Designer
Resolution
When using the Vijeo Designer Link Variable feature to link RSLogix5000 *.L5K file, one will only be able to import the tags that are declared in the Logix application and not the bit extraction of the tag.
The work around would be to manually create those tags as new Variables in Vijeo Designer.
To extract that bit, you will have to manually create the tags in Vijeo Designer as Program:MainProgram.tagname.x as the Device Address (where x is the bit 0 to 15 location for a program scope tag).
Does Vijeo Designer link to individual bits from an INT or DINT using the RSLogix 5000 L5K file?
Product Line
Vijeo Designer
Resolution
When using the Vijeo Designer Link Variable feature to link RSLogix5000 *.L5K file, one will only be able to import the tags that are declared in the Logix application and not the bit extraction of the tag.
The work around would be to manually create those tags as new Variables in Vijeo Designer.
To extract that bit, you will have to manually create the tags in Vijeo Designer as Program:MainProgram.tagname.x as the Device Address (where x is the bit 0 to 15 location for a program scope tag).
Released for: Schneider Electric Saudi Arabia


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.