Issue
Unable to connect to the G3200 gateway
Product Line
G3200
Resolution
The G3200 supports up to 6 simultaneous IEC61850 and 4 Modbus TCP/IP connections at one time. If this maximum number of connections is met, no other connections are allowed to the device.
Unable to connect to the G3200 gateway
Product Line
G3200
Resolution
The G3200 supports up to 6 simultaneous IEC61850 and 4 Modbus TCP/IP connections at one time. If this maximum number of connections is met, no other connections are allowed to the device.
Released for: Schneider Electric Saudi Arabia






Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.