Issue:
ATV312 Sleep function configuration
Product Line:
All ATV312 Drives
Environment:
All model numbers, all serial numbers
Cause:
Sleep function
Resolution:
Yes.
TLS is a low speed time out. If the drive is maintaining low speed (LSP) for the amount of time you set under TLS (in seconds), then will cause the drive to go to sleep.
It will wake up and run when commanded faster than LSP.
Press Enter (press on the dial) and scroll down (turn the dial clockwise) to SET menu.
Press Enter and scroll down to TLS parameter.
Press Enter to view current setting and to make changes.
Press Enter to save changes.

ATV312 Sleep function configuration
Product Line:
All ATV312 Drives
Environment:
All model numbers, all serial numbers
Cause:
Sleep function
Resolution:
Yes.
TLS is a low speed time out. If the drive is maintaining low speed (LSP) for the amount of time you set under TLS (in seconds), then will cause the drive to go to sleep.
It will wake up and run when commanded faster than LSP.
Press Enter (press on the dial) and scroll down (turn the dial clockwise) to SET menu.
Press Enter and scroll down to TLS parameter.
Press Enter to view current setting and to make changes.
Press Enter to save changes.
Released for: Schneider Electric Saudi Arabia


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.