Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What type of material is used for Flite construction?
Flite is constructed using high grade Industrial components as detailed below
  1. Enclosure (part in grey color) : PEHD or High Density Polyethylene is used in the manufacturing of the Flite Enclosure
  2. Transparent  glass part : LEXAN
  3. Attachement Claws : Polyamide for the clip and an Elastomer for the brake block.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre