Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do we have fuse on our PCB board in the base station, if customer wiring the wrong Voltage it will protect the base station. If we have, can you give me the picture to show which one is Fuse. And if the fuse was burned, how to change a new one. Because th
There are fuses in our base. It is not possible for the customer to change them. By the way you have to use a external protection as mentioned in the User Guide and User Manual.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre