{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there system words available in the M340 to help me troubleshoot the READ_VAR and WRITE_VAR communication block?
There are a few system words to help.

%SW90 provides the maximum number of requests that the PLC can handle.
%SW86 indicates the number of messages being refused.  It should always be at 0.

Schneider Electric Saudi Arabia