Issue
In AOS v6.4.0/rpdu2g v6.4.0, the AP8966 Rack Power Distribution Unit (PDU) shows incorrect bank to phase relationships. (The silkscreen markings on the unit's chassis are correct.)
Correct:
Incorrect (currently shown within the product's interfaces):
Product Line
Environment
Cause
This issue is caused by a firmware bug within the Rack PDU Network Management Card (NMC) Firmware.
Resolution
It is recommended that the user refer to the accurate silkscreen markings directly on the chassis of the Rack PDU itself in order to understand the correct bank to phase relationships in order to correctly balance loads across phases. Alternatively, refer to the "Correct" screenshot above for accurate phase to bank relationship information. No measurements provided are incorrect, just the phase to bank information shown within the NMC interfaces.
This issue will be fixed in rpdu2g application v6.4.4 (and higher), available in September, 2016.
In AOS v6.4.0/rpdu2g v6.4.0, the AP8966 Rack Power Distribution Unit (PDU) shows incorrect bank to phase relationships. (The silkscreen markings on the unit's chassis are correct.)
Correct:
Incorrect (currently shown within the product's interfaces):
Product Line
- Rack Power Distribution
- AP8966 model only
Environment
- All serial numbers
- Firmware version AOS 6.4.0/rpdu2g v6.4.0
Cause
This issue is caused by a firmware bug within the Rack PDU Network Management Card (NMC) Firmware.
Resolution
It is recommended that the user refer to the accurate silkscreen markings directly on the chassis of the Rack PDU itself in order to understand the correct bank to phase relationships in order to correctly balance loads across phases. Alternatively, refer to the "Correct" screenshot above for accurate phase to bank relationship information. No measurements provided are incorrect, just the phase to bank information shown within the NMC interfaces.
This issue will be fixed in rpdu2g application v6.4.4 (and higher), available in September, 2016.
Released for: Schneider Electric Saudi Arabia


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.