Issue:
Retrieving surveillance clips in StruxureWare Data Center Expert.
Product Line:
Environment:
Cause:
This is for customers that require assistance in retrieving NetBotz camera clips in DCE
Resolution:
NOTE: The Netbotz 750/755 appliances do not include images in the alert notification themselves. Images can be cross referenced and are available in Data Center Expert Surveillance.
1) Open the DCE Client and go to the Surveillance perspective.
2) Select a device group in the Device Groups pane.
3) Within the Thumbnails pane, you will see the camera thumbnails for your NetBotz Appliances that are in the group you selected.
NOTE: If a thumbnail shows a red circle with a cross-line through it, the camera has not been licensed for surveillance. See knowledge base FA297815 for instructions.
4) Right-click on the camera and select Retrieve Clips.
NOTE: Clips are stored according to the NetBotz Appliance date/time, not the DCE Appliance date/time.
5) Within the Choose Date section, select either Relative or Date Range.
NOTE: If using relative, ensure that the date/time on the DCE Appliance is accurate, as it will be used as a reference point.
6) Select Retrieve Clips and a list of clips during that time frame will show within the list.
7) You can select a clip and then select View.
NOTE: You can also tag, export, or delete clips.
Retrieving surveillance clips in StruxureWare Data Center Expert.
Product Line:
- StruxureWare Data Center Expert (DCE)
- NetBotz
Environment:
- StruxureWare Data Center Expert (DCE)
- NetBotz discovered by DCE and licensed for surveillance
Cause:
This is for customers that require assistance in retrieving NetBotz camera clips in DCE
Resolution:
NOTE: The Netbotz 750/755 appliances do not include images in the alert notification themselves. Images can be cross referenced and are available in Data Center Expert Surveillance.
1) Open the DCE Client and go to the Surveillance perspective.
2) Select a device group in the Device Groups pane.
3) Within the Thumbnails pane, you will see the camera thumbnails for your NetBotz Appliances that are in the group you selected.
NOTE: If a thumbnail shows a red circle with a cross-line through it, the camera has not been licensed for surveillance. See knowledge base FA297815 for instructions.
4) Right-click on the camera and select Retrieve Clips.
NOTE: Clips are stored according to the NetBotz Appliance date/time, not the DCE Appliance date/time.
5) Within the Choose Date section, select either Relative or Date Range.
NOTE: If using relative, ensure that the date/time on the DCE Appliance is accurate, as it will be used as a reference point.
6) Select Retrieve Clips and a list of clips during that time frame will show within the list.
7) You can select a clip and then select View.
NOTE: You can also tag, export, or delete clips.
Released for: Schneider Electric Saudi Arabia








Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.