{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which is the consumption of the BCPM main boards and the adapter boards?
The current draw of the BCPM main board with all four daughter boards is approximately 30mA.
The board is fused at 500mA so even in case of catastrophic failure it could not draw more than that.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.