{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do we offer a drive with 120V input and 120V output?
Issue:
Drive selection for 120V input and 120V output

Product Line:
ATV12

Environment:
120v output

Cause:
n/a

Resolution:
No, the only 120v input drive we have is the ATV12 drive and the output to this drive is 230v (3-phase).  No 120v output from any of our drives.

Schneider Electric Saudi Arabia