{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the drive relays on Process Drives be assigned to indicate transition between local controls and remote controls?
Issue:
Wants to program the drive relays  to be assigned to indicate transition between local and remote controls.

Product Line:
ATV630

Environment:
All Serial numbers

Cause:
Need to know if local or remote controls

Resolution:
Yes. First, set the HMI Cmd to Bumpless  [Complete setting> Command and Reference> HMI Cmd = bumpless]
then Goto [Complete setting> Input/Output > Relay Configuration]
Set R3 to HMI Cmd (BMP:Control via the Graphic Display Terminal is active).

Schneider Electric Saudi Arabia