Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find a manual and ESI file for VW3A3601 EtherCAT Module?
Issue:
Manual and ESI file for Altivar drives using EtherCAT option card

Product Line:
ATV32
ATV320
ATV340
ATV900


Environment:
All

Cause:
EtherCAT Connectivity

Resolution:

The EtherCAT option card manuals are specific to each drive family they are being installed in.  See the following links:
ATV32: https://www.se.com/ww/en/download/document/S1A28703/
ATV320: https://www.se.com/ww/en/download/document/NVE41315/
ATV340: https://www.se.com/ww/en/download/document/NVE61686/
ATV900: https://www.se.com/ww/en/download/document/NHA80946/

The ESI files for the Module VW3A3601 are dependent on the version of the option card:
V1.01 (ATV32 only): https://www.se.com/ww/en/download/document/ATV32_EtherCAT_ESI/
V1.03 (ATV32 only)" https://www.se.com/ww/en/download/document/ATV32 EtherCAT ESI file_V103/
V1.09 (Min FW version for ATV320): https://www.se.com/ww/en/download/document/EthCAT_VW3A3601_V109/
V1.12: https://www.se.com/ww/en/download/document/EthCAT_VW3A3601_V112/
V1.13: https://www.se.com/ww/en/download/document/EtherCAT_ESI_VW3A3601_V113/
V1.14: https://www.se.com/ww/en/download/document/EtherCAT_ESI_V1.14/

As additional versions are released the website will be update to include them.

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings