undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Are there instructions available showing how to install NetShelter seismic mounting brackets onto different floor types?
Issue:
The NetShelter seismic mounting brackets need to be mounted to the floor. There are different floor types.

Product Line:
NetShelter SX

Environment:
All models, all serial numbers.

Cause:
The NetShelter seismic mounting brackets installation manuals only show mounting to the cabinet, not the floor.

Resolution:
Using the pallet bracket or AR7701 the NetShelter SX can be installed per IBC Low Seismic Area and Moderate Seismic Area onto a concrete slab, concrete fill over metal deck, raised composite floor concrete filled metal deck, and raised composite floor concrete slab.
Reference the IBC Seismic Calculations for NetShelter SX for instructions: http://www.apc.com/salestools/SNEL-8C7UQS/SNEL-8C7UQS_R6_EN.pdf
An updated document can be loaded off the APC website of any NetShelter SX cabinet under the Documentation tab.

Using AR7701A-S the NetShelter SX can be installed per OSHPD onto a concrete slab, and concrete fill over metal deck.
Reference the OSHPD structural drawings for NetShelter SX for instructions: http://www.apc.com/salestools/JKUR-ATJL8V/JKUR-ATJL8V_R0_EN.pdf
The AR7701A-S can also be installed to meet IBC High Seismic Area using these instructions:
http://www.apc.com/salestools/SNEL-8C7UQS/SNEL-8C7UQS_R6_EN.pdf


Schneider Electric Saudi Arabia

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: