Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can we comply the specification requirement of transient over torque is 200%?
As per the catalog specification, if we select the heavy duty drive (ATV630 or ATV930) the maximum transient over current is 150%.

But it is given if you used a motor with one power rating lower. For example, if the drive is a 15kW, to have 150% of over current, the motor used is maximum an 11kW (for standard power rating asynchronous motor). Otherwise, if you need for a 15kW motor, over current of 150% you have to used an 18.5kW drive (Pn+1).
In the case of 200% of over current, the principal is similar. I made an example in the excel file in attachment ("example drive selection.xlsx") and in that case drive have to be taken twice the power of the motor (Pn+2).

Schneider Electric Saudi Arabia

Attachment(s)
example drive selection.xlsx [128.86 KB]