The RealStream Lift Station allows the submersible pump sensor relays like temperature and seal failure to be fed directly into the controller, which will automatically stop the pump if configured.
Released for: Schneider Electric Saudi Arabia


Our Brands
Welcome to the Schneider Electric Website
Discuss this topic with experts