Issue:
Using VW3A1101 keypad on multiple ATV212 drives.
Product Line:
ATV212
Environment:
Keypad
Cause:
n/a
Resolution:
Response from France:
The VW3A1101 keypad used on ATV212 is just like a mirroring display with a long label. You can see it because; the local ATV212 display will change in the same time, that the keypad displays.
VW3A1101 keypad + ATV212 does not offer the same characteristics (configuration saving, Multidrop, HMI personalization, menu organization, etc.), like with VW3A1101 + ATV320 or ATV61 or ATV71.
So the Multidrop/Multipoint is not possible with the ATV212 and VW3A1101.
There is a mistake in the catalog. Request has been made to correct it ( 1/2/19).
Using VW3A1101 keypad on multiple ATV212 drives.
Product Line:
ATV212
Environment:
Keypad
Cause:
n/a
Resolution:
Response from France:
The VW3A1101 keypad used on ATV212 is just like a mirroring display with a long label. You can see it because; the local ATV212 display will change in the same time, that the keypad displays.
VW3A1101 keypad + ATV212 does not offer the same characteristics (configuration saving, Multidrop, HMI personalization, menu organization, etc.), like with VW3A1101 + ATV320 or ATV61 or ATV71.
So the Multidrop/Multipoint is not possible with the ATV212 and VW3A1101.
There is a mistake in the catalog. Request has been made to correct it ( 1/2/19).
Released for: Schneider Electric Saudi Arabia