Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
NetBotz 250 | Network Port Light Indicators
Issue:
Description of the Network Port lights (Link/Status) on NetBotz 250

Product Line:
NetBotz Rack Monitor 250 (NBRK0250)

Environment:
NetBotz Rack Monitor 250 (all versions)

Resolution:

Link (10/100) LED
The LED on the right of any network port indicates the network status.
ConditionDescription
OffOne or more of the following situations exist:
  • The Rack Monitor 250 is not receiving input power.
  • The cable that connects the Rack Monitor 250 to the network is disconnected or not functioning properly.
  • The Rack Monitor 250 is turned off or not operating correctly. It may need to be repaired or replaced. Contact Customer Support at www.apc.com/support.
Solid GreenThe Rack Monitor 250 is connected to a network operating at 10 Megabits per second (Mbps).
Solid OrangeThe Rack Monitor 250 is connected to a network operating at 100 Mbps.
Flashing GreenThe Rack Monitor 250 is receiving or transmitting data packets at 10 Mbps.
Flashing OrangeThe Rack Monitor 250 is receicing or transmitting data packets at 100 Mbps.

Status LED
The LED on the left side of any network port indicates the status of the appliance.
ConditionDescription
OffOne of the following situations exists:
  • The Rack Monitor 250 is not receiving input power.
  • The Rack Monitor 250 is not operating properly. It may need to be repaired or replaced. Contact Customer Support at www.apc.com/support.
Solid GreenThe Rack Monitor 250 has valid TCP/IP settings.
Flashing GreenThe Rack Monitor 250 does not have valid TCP/IP settings.1
Flashing OrangeThe Rack Monitor 250 is making BOOTP requests.
Rapidly Flashing GreenA user initated a LED blink test from the user interface.
Alternately flashing green and orangeIf the LED is flashing slowly, the Rack Monitor 250 is making DHCP requests.1
If the LED is flashing rapidly, the Rack Monitor 250 is starting up.

1 If you do not use BOOTP or DHCP server, the network settings will need to be configured manually.  Instructions for manually configuring TCP/IP settings can be found in knowledge base NetBotz 250 | Configuring Network Settings .

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: