Issue:
Captured clips shows duration and frame rate as per previous video capture settings on NetBotz 750 / 755
Product Line:
NetBotz 700 series
Environment:
Nebotz 5.2.3 firmware and prior
NBRK0750
NBWL0755
StruxureWare Data Center Expert
Cause:
This issue may be seen in StruxureWare Data Center Expert's surveillance data for the 700 series appliance with the issue.
Steps to recreate the issue:
1. Set both pre capture and post capture time to 30 seconds
2. Set frame rate/second to 30 seconds (Under camera settings)
3. Trigger an alarm with clip capture attached
4. Captured clip contains around 330 frames and duration 45 seconds
5. Resolve the alarm (Do not delete the alarm configuration)
6. Change both pre capture and post capture time to 2 seconds
7. Set frame rate/second to 2 seconds(Under camera settings)
8. Trigger an alarm with clip capture attached
9. Captured clip contains around 557 frames and duration 1 minute
Resolution:
1. Delete the alarm configurations in which clip capture option selected
2. Create a new alarm configuration with clip capture option selected
3. In the triggered alarm, Captured clip should now contain around 8 frames and duration 3 seconds.
This issue is slated to be fixed in BotzWare 5.3
Captured clips shows duration and frame rate as per previous video capture settings on NetBotz 750 / 755
Product Line:
NetBotz 700 series
Environment:
Nebotz 5.2.3 firmware and prior
NBRK0750
NBWL0755
StruxureWare Data Center Expert
Cause:
This issue may be seen in StruxureWare Data Center Expert's surveillance data for the 700 series appliance with the issue.
Steps to recreate the issue:
1. Set both pre capture and post capture time to 30 seconds
2. Set frame rate/second to 30 seconds (Under camera settings)
3. Trigger an alarm with clip capture attached
4. Captured clip contains around 330 frames and duration 45 seconds
5. Resolve the alarm (Do not delete the alarm configuration)
6. Change both pre capture and post capture time to 2 seconds
7. Set frame rate/second to 2 seconds(Under camera settings)
8. Trigger an alarm with clip capture attached
9. Captured clip contains around 557 frames and duration 1 minute
Resolution:
1. Delete the alarm configurations in which clip capture option selected
2. Create a new alarm configuration with clip capture option selected
3. In the triggered alarm, Captured clip should now contain around 8 frames and duration 3 seconds.
This issue is slated to be fixed in BotzWare 5.3
Released for: Schneider Electric Saudi Arabia








Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.