Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
StruxureWare Data Center Expert shows duplicate sensors with values as "Unplugged" for NetBotz 750/755
Issue:
StruxureWare Data Center Expert (DCE) shows duplicate sensors with values as "Unplugged" for NetBotz 750/755 after reset of the NetBotz unit

Product Line:
NetBotz

Environment:
StruxureWare Data Center Expert (DCE)
NetBotz NBRK0750 / NBWL0755
Potentially any version.


Cause:
When a NetBotz 5 discovers devices plugged into it or into Pods plugged into it, each device is given a unique identifier in the database. This identifier is used as part of the algorithm to generate the sensor's unique OID in the MIB. DCE walks the MIB and stores the sensors and their state. If the device has a factory reset run on it however, the database is deleted and along with all of the sensor IDs. As the sensors get rediscovered they end up in the database but will generally have different IDs. When DCE walks the MIB it sees the new sensors and values and they are displayed in DCE. However, it knows of the old sensors so it treats them as unplugged.

Resolution:
It is suggested that you remove the appliance from DCE prior to resetting the appliance. Once reset, re-add the NetBotz to DCE.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings