Issue:
Use default P3 driver in Profile editor.
Simulate alarm for this tag which is in the default driver but no alarm show up in PSO2020.
Simulate alarm in Easergy P3 and related alarm can be read by 3td party modbus test tool.
Request:
Response:
01 03 0A 04 C1 XXXX 04C1 whichi is for (Protection 50/51 Alarm) 1217
Cause: The root cause of this issue is the onboard alarms are disabled by default.
Answer:
The driver supports the download of on-board event logs. The device driver polls the device and checks for new log entries at regular intervals. The default polling interval is 500 m seconds.
Event log feature is disabled by default. To enable, set the parameter in the citect.ini file.
[Easergy.(cluster name).(equipmentName)]
EventLogEnabled=1.
Use default P3 driver in Profile editor.
Simulate alarm for this tag which is in the default driver but no alarm show up in PSO2020.
Simulate alarm in Easergy P3 and related alarm can be read by 3td party modbus test tool.
Request:
Response:
01 03 0A 04 C1 XXXX 04C1 whichi is for (Protection 50/51 Alarm) 1217
Cause: The root cause of this issue is the onboard alarms are disabled by default.
Answer:
The driver supports the download of on-board event logs. The device driver polls the device and checks for new log entries at regular intervals. The default polling interval is 500 m seconds.
Event log feature is disabled by default. To enable, set the parameter in the citect.ini file.
[Easergy.(cluster name).(equipmentName)]
EventLogEnabled=1.
Released for: Schneider Electric Saudi Arabia


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.