Issue:
The PowerChute service does not automatically restart following an upgrade to OpenJDK 16.
Product Line:
PowerChute Business Edition v10.0.2
Environment:
SUSE Linux Enterprise Server 15 SP2
Solution:
Follow the below steps to resolve the issue:
1. Open the PBEAgent file located in the /usr/bin directory.
2. Search for âjdk-16(2)â in line 75. Refer to the below screenshot as an example.
3. Remove â(2)â. For example, update this line to read: 'JAVA_RUNTIME=/opt/APC/PowerChuteBusinessEdition/Agent/../jdk-16/jre/bin/java'
4. Navigate to the PowerChuteBusinessEdition directory and delete the empty âjdk-16â folder. Modify the name of the âjdk-16(2)â directory to âjdk-16â.
5. Manually restart the PowerChute service. To restart enter /etc/init.d/PBEAgent restart.
Released for: Schneider Electric Saudi Arabia


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.