Issue:
Customer has a ATV630U55N4 and Modbus TCP/IP and cannot change his I/O scanner table, in Somove. He was trying to add Register 3204 to his scanner table and it was grayed out and could not
add it. He was positive the drive was not running. Tried power cycling the drive a couple of times and still could not add Register 3204.
Product Line:
ATV630
Environment:
Modbus TCP/IP
Cause:
n/a
Resolution:
The I/O table is always grayed out, but it is possible to add registers. Check with the customer to see how he is trying to add the registers ?
If he is trying to double click, that will not work. He needs to right click on the mouse and then click on add. See attachment.
Released for: Schneider Electric Saudi Arabia


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.