Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Cannot Insert Duplicate Key

Issue

SQL Server Management Studio throws the following error when assigning data to a location where data already exists, ex. reassigning data to a source that is already populated when performing the functions in How to move historical data from an existing device to another device in Power Monitoring Expert | Schneider Electric USA

"Cannot insert duplicate key row in object 'dboDataLog2' with unique index 'CIX_DataLog2_SourceID_QuantityID_TimestampUTC'. The duplicate key value is (...)"

error

Product Line

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment

Microsoft SQL Server Management Studio

Cause

The device to which data is being assigned already has existing entries for the specific time stamps included in the script. This may happen due to an overlap in time between disabling and enabling the two devices that data is being transferred between. In the following example the error is seen when trying to insert data to the source in the first column from 1/28/2025 8:15:00 AM onwards.

data

Resolution

Be sure to take an updated backup of the ION_Data database before making these changes

Remove the existing data, which is unwanted and intended to be replaced by using the following scripts, use desired SourceID (verify from [ION_Data].[dbo].[Source]) and TimestampUTC based on the system.

DELETE FROM [ION_Data].[dbo].[DataLog2] where SourceID = 9 and QuantityID = 69 and TimestampUTC > '2022-09-14' and TimestampUTC <  '2022-09-15'

Proceed with https://www.se.com/us/en/faqs/FA271539/

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings