Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

We are an OCP Platinum Member

Started in 2011 by Facebook, Intel, Rackspace and Goldman Sachs, The Open Compute Project (OCP) is a collaborative community focused on redesigning hardware technology to efficiently support the growing demands on compute infrastructure. As a Platinum Member of OCP, Schneider Electric is taking a leadership role in shaping tomorrow's data centres.
Learn more

An OCP Inspiredâ„¢ solution

Compatible with Open Compute V2 rack specification, this 2OU, 12VDC rack PSU has earned OCP Inspiredâ„¢ recognition. Major features include:
  • 15 kW N+1 or 9 kW 2N configurations
  • Input ATS for dual feed
  • Can monitor up to 2 BBU shelves
  • Software defined power compatible
For more information or to order, use the form at the bottom of this page.
OCP Inspired PSU Gemini

Data Centre IT Pod Specs

Optimising POD design creates an architecture that's scalable and repeatable, simplifies power and cooling infrastructure, facilitates roll-in and out OCP racks and maximises white space.

Need help?

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

 opens in new window

Help Centre

Find support resources for all your needs, in one place.