Solution with the best functionality/cost ratio for simple machines, up to 1 circuit for 2 compressors
Solution
With the all-in-one Harmony SCU, the architecture is a cost-efficient solution.
Simple, standard boosters are the first step toward automation, moving away from traditional relay architectures. Single-drive boosters can be used in single- or multi-drive mods.
Benefits
> Capable of managing multiple pumps using one drive
> Maintains constant pressure in the system with PID, pump stage and de-stage-related functions
> Diagnostic features for easy maintenance
> Embedded booster and pumps protection
> Operates smaller (auxiliary) pumps to maintain lower flow requirement