How to establish Ethernet communication between Twido controller and Zelio Logic with Ethernet extension SR3NET01BD.
It is possible to establish Ethernet communication between a Twido controller and Zelio Logic with Ethernet extension SR3NET01BD.
In this communication, user have to remember that Zelio logic relay SR3 series(24VDC Supply)+ Ethernet extension SR3NET01BD will
always act as Slave(Server) on Ethernet network and Twido Controller will be the Master(Client)on Ethernet network).Refer to attached file for
the complete procedure with sample programs.