When using Vijeo XD to program HMISTO7xx, ensure you do not use large resolution images for the application. Otherwise, the panel changes will occur slowly at runtime. This is because the HMI needs to downsize the image during runtime and this takes CPU time.
To avoid this issue, downsize the image resolution before adding it to the application.