Våra varumärken

Impact-Company-Logo-English Black-01-177x54

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Video: How do you program the ATV212 or ATV21 drive to run in reverse mode?
Issue:
Adding a reverse mode in ATV212 or ATV21 drives

Product Line:
Altivar ATV212 & ATV21

Environment:
All models

Cause:
Requirement to program logic input R to run the motor in reverse.

Resolution:
Programming example for 2 wire control with logic input R being your reverse logic input command.

Go to the extended menu, F---  and press enter.
F112 = 3  logic input R (Reverse command)
F311 = 0  (Motor rotation direction command)
Please note, if you do not program F311 = 0, the drive will not run in reverse.

F311 parameter

Note:  Parameter Fr = 2 will allow run reverse command when in Local mode.

Schneider Electric Sverige

Bilagor
atv212_programming_manual_en_s1a53838_02.pdf [3.58 MB]