Sök bland vanliga frågor (FAQ)
{"searchBar":{"inputPlaceholder":"Sök med nyckelord eller ställ en fråga","searchBtn":"Sök","error":"Ange ett sökord"}}
Osisense XC special - Technical difference between the XRBA41100 & XRBA41102525 screw limit switches
Both references XRBA41100 & XRBA411002525 use the same contact number (4 contacts) and the same gearbox (reduction ratio 13/1).
The difference is concerning only the cam arrangement of the 4 contacts. In the standard XRBA41100 switch, the cam arrangement by default is attached. Attached too the XRBA41102525 contact arrangement
The difference is concerning only the cam arrangement of the 4 contacts. In the standard XRBA41100 switch, the cam arrangement by default is attached. Attached too the XRBA41102525 contact arrangement
Bilagor
Var det här till hjälp?
Utforska mer
Produktfamilj
Utforska mer
Produktfamilj