Sök bland vanliga frågor (FAQ)
{"searchBar":{"inputPlaceholder":"Sök med nyckelord eller ställ en fråga","searchBtn":"Sök","error":"Ange ett sökord"}}
Osisense XC - Can I use the XE2SP2151 contacts to change those of the XCKML102 dual contact switch?
The XE2SP2151 contacts cannot replace those of the XCKML102 dual contact switch, even if they look similar. The XCKML102 contacts are special, pre-adjusted in the ZCKML1 body and adjusted after the head assembling in the body. For maintenance, the best is to select a complete body pre-adjusted in the factory : ZCKML1 for the XCKML102 limit switch, available to order in March 2022. However XCKML contacts are available to order separately : snap contacts XESP2151L, slow break XE2NP2151L. Please refer to the attached picture
Published for:Schneider Electric Sverige
Bilagor
Var det här till hjälp?
Utforska mer
Utforska mer